DIN#.FILTER

Description

This parameter gets or sets the digital input filter. The digital filter blocks input changes (rising or falling edges) until the minimum pulse width is exceeded. The +/- tolerance listed is the sample period (uncertainty) of the filter.

Value Description Min Pulse Width Typical Use
0 Unfiltered >40ns RS485 inputs
4 Ultra fast

>240ns

+/- 40ns

Fast Optos

1 Fast

>10.24 µs

+/- 0.64 µs

Fast Optos
2 Standard

>163µs

+/- 10.24µs

Slow Optos
3 Slow

>2.62ms

+/- 0.16384ms

Mechanical switch

Examples

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 4
Default Value

Depends on DIN:

4 for DIN1-2

2 for DIN3-12

Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DIN1.FILTER

3590h

02h

Unsigned8

-

-

Read/Write

No

DIN2.FILTER

3591h

02h

Unsigned8

-

-

Read/Write

No

DIN3.FILTER

3592h

02h

Unsigned8

-

-

Read/Write

No

DIN4.FILTER

3593h

02h

Unsigned8

-

-

Read/Write

No

DIN5.FILTER

3594h

02h

Unsigned8

-

-

Read/Write

No

DIN6.FILTER

3595h

02h

Unsigned8

-

-

Read/Write

No

DIN7.FILTER

3596h

02h

Unsigned8

-

-

Read/Write

No

DIN8.FILTER

3597h

02h

Unsigned8

-

-

Read/Write

No

DIN9.FILTER

3598h

02h

Unsigned8

-

-

Read/Write

No

DIN10.FILTER

3599h

02h

Unsigned8

-

-

Read/Write

No

DIN11.FILTER

359ah

02h

Unsigned8

-

-

Read/Write

No

DIN12.FILTER

359bh

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DIN1.FILTER

20100

4E84

Unsigned8

Read/Write

-

DIN2.FILTER

20101

4E85

Unsigned8

Read/Write

-

DIN3.FILTER

20102

4E86

Unsigned8

Read/Write

-

DIN4.FILTER

20103

4E87

Unsigned8

Read/Write

-

DIN5.FILTER

20104

4E88

Unsigned8

Read/Write

-

DIN6.FILTER

20105

4E89

Unsigned8

Read/Write

-

DIN7.FILTER

20106

4E8A

Unsigned8

Read/Write

-

DIN8.FILTER

20107

4E8B

Unsigned8

Read/Write

-

DIN9.FILTER

20108

4E8C

Unsigned8

Read/Write

-

DIN10.FILTER

20109

4E8D

Unsigned8

Read/Write

-

DIN11.FILTER

20110

4E8E

Unsigned8

Read/Write

-

DIN12.FILTER

20111

4E8F

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DIN1.FILTER

20100

Unsigned8

Read/Write

-

DIN2.FILTER

20101

Unsigned8

Read/Write

-

DIN3.FILTER

20102

Unsigned8

Read/Write

-

DIN4.FILTER

20103

Unsigned8

Read/Write

-

DIN5.FILTER

20104

Unsigned8

Read/Write

-

DIN6.FILTER

20105

Unsigned8

Read/Write

-

DIN7.FILTER

20106

Unsigned8

Read/Write

-

DIN8.FILTER

20107

Unsigned8

Read/Write

-

DIN9.FILTER

20108

Unsigned8

Read/Write

-

DIN10.FILTER

20109

Unsigned8

Read/Write

-

DIN11.FILTER

20110

Unsigned8

Read/Write

-

DIN12.FILTER

20111

Unsigned8

Read/Write

-